Single-Pair Ethernet Connectors

Ethernet was commercially introduced in the early 1980’s and was soon after standardized in 1983 according to the IEEE 802.3 specification. In today’s environment, where ethernet has far surpassed its original intention of just connecting computer to computer systems, we (KYOCERA AVX) have seen the Industrial IoT and Automotive Ethernet market require faster data transmission, while still providing a ruggedized connection system. In order to provide customers with the best solution, we are at the forefront of the development of single pair Ethernet connectors.